Modbus Mapping


What you will find in this section:

  1. Modbus mapping
  2. Related topics

 

Modbus mapping

 

The EMpro offers the option of mapping various registers to a defined contiguous Modbus register area.

This allows multiple registers from different address spaces to be retrieved in a single read command.

  • The contiguous area comprises 125 registers, as this is the maximum number of registers that can be read in one read command
  • The mapping is limited to process data, as this is considered relevant for this application
  • The mapping is implemented at register level, independent of data points and data types.

The 125 mapped register addresses - starting at register 57.600 (Hex: 0xE100) – can only be read by the user.

The assignment of content for these registers takes place in the 125 registers starting at 57.344 (Hex: 0xE000) and is also possible via the web server. Configuration via the display is not provided.

 

Example:

The system conductor voltage (register: 32829), the system current (register: 32825), the frequency (register 32.780) and the total active power (register 32.790) are to be received via a read command.

  • For this it is necessary to store the registers to be mapped in the allocation registers. The number of registers to transfer a value depends on the data type. All register addresses must be stored in the allocation registers.

57.344: 32.829

57.345: 32.830

57.346: 32.825

57.347: 32.826

57.348: 32.780

57.349: 32.781

57.350: 32.790

57.351: 32.791

57.352: 16.452

  • The format of query must then be set according to the configured input data in the mapped register addresses.

57.600 → 32 Bit Float (little endian byte swap)

57.602 → 32 Bit Float (little endian byte swap)

57.604 → 32 Bit Float (little endian byte swap)

57.606 → 32 Bit Float (little endian byte swap)

57.608 → 16 Bit Integer (little endian byte swap)

Menu: „Settings, Modbus Mapping“
Menu: „Settings, Modbus Mapping“


EMpro online documentation
Published/reviewed: 2026-07-10, en revision 004, Version history